Resources

Real People. Real Service.
Help Face
Need a little help?
Email
Response by Mon
Plumbing Supplies
Have a plumbing problem? We have a plumbing solution. From minor issues to major installations, our product videos, sizing calculators, and in-depth articles can help you save time, money, and stress on your next plumbing job.

Videos

Show Less
Sizing Your Grease TrapPlay Icon
Sizing Your Grease Trap
Choosing Between Tank and Tankless Water HeatersPlay Icon
Choosing Between Tank and Tankless Water Heaters
Types of Water HeatersPlay Icon
Types of Water Heaters
Shopping for a MANABLOCPlay Icon
Shopping for a MANABLOC
Dielectric UnionsPlay Icon
Dielectric Unions
Comparing PVC FittingsPlay Icon
Comparing PVC Fittings
Venting for Boilers and Water HeatersPlay Icon
Venting for Boilers and Water Heaters
Spigot vs. Socket PVC FittingsPlay Icon
Spigot vs. Socket PVC Fittings
Manifolds for Plumbing SystemsPlay Icon
Manifolds for Plumbing Systems
Indirect Water HeatersPlay Icon
Indirect Water Heaters
Water Heater AdaptersPlay Icon
Water Heater Adapters
Sizing Tankless Water HeatersPlay Icon
Sizing Tankless Water Heaters
Anode Rode ReplacementPlay Icon
Anode Rode Replacement
Differences Between Swing and Spring Check ValvesPlay Icon
Differences Between Swing and Spring Check Valves
Stop ValvesPlay Icon
Stop Valves
Ball ValvesPlay Icon
Ball Valves
Expansion Tanks (How it Works)Play Icon
Expansion Tanks (How it Works)

Calculators

Grease Trap CalculatorGrease Trap CalculatorExpansion Tank Size CalculatorExpansion Tank Size Calculator

Articles

Valves

+
There are many different valves available to aid in the control of plumbing and heating systems. The list below includes some of the most common valves used in plumbing systems and describes when and why they are used.
Ball Valves are the most common valve used in plumbing and heating systems. A ball valve is opened by turning a handle that is attached to a ball inside the valve. The ball has a hole or port in the middle of it that allows water to flow through when it is in line. When the valve is closed, the hole turns perpendicular to the ends of the valve and flow is stopped. The term full port refers to the fact that the hole in the ball is the same size as the pipeline and does not restrict flow.
Boiler drains are horizontal faucets that have male or female threads that are angled perpendicular to the bottom of the valve. They are called boiler drains because they were designed to drain water from a boiler to remove sediment. Boiler drains may also be used for a laundry tub to hookup to a washing machine.
Check valves ensure that water is only able to flow through in one direction and not back in the other direction. They are often used in plumbing and heating systems. These valves come in spring loaded and swing varieties.
Frost free sillcocks are used to prevent frozen pipes in a residential plumbing application. They accomplish this by keeping the valve inside the house and away from the cold. Frost free sillcocks are most commonly used for garden hoses.
Gas ball valves are used in residential applications to aid in the control of natural gas and liquid propane. They feature a ball and handle that will allow the gas line to be turned off.
Gate valves open by lifting a rectangular wedge out of the water line. Gate valves are often used for regulating the flow of water. However, some of these valves are designed to either be fully opened or closed.
Sillcocks are faucets that are designed to be installed horizontally on the outside wall. These are commonly used for connecting to a hose in residential applications.

Grease Traps

+
Every restaurant needs a grease trap to ensure that water flows properly and that pipes do not get clogged. Some home cooks will install a grease trap if there is a level of grease too high for the standard “dump it in a coffee can” method. Grease traps are sized by the amount of liquid that will be flowing through them. The best way to gauge this is through the size of the sink or sinks that you are using the grease trap for. The capacity of how much grease the trap will hold is less important because you can always clean the trap more or less frequently if needed. What is most important is that the grease trap can handle the maximum flow coming through at any time. The flow consists of water, grease, and whatever else comes down the sink. A grease trap works to separate out the water from everything else and allow the water to continue flowing through while keeping the grease trapped under your sink. In order to determine what size grease trap to purchase for your sink, you can use our Grease Trap Calculator. This calculator takes into account the length, width, and height of your sink as well as if there will be a very low level of grease or not. Be conservative when determining whether or not there is a “very low level of grease.” It is better to have a bigger grease trap than a grease trap that cannot handle the amount of fluid passing through.

Backflow Preventers

+
The purpose of a backflow preventer is to protect the public water supply. Public water goes to each and every facility (house, office, farm, etc.) in a water company's reach. Once that public water enters a facility, it cannot be returned back to the public supply to go somewhere else. Backflow preventers are needed for irrigation, drinking water, and fire water.
There are 4 types of parts you might need to repair a backflow preventer. If there is an issue with any of the rubber parts, you can get a complete rubber kit. Also available are a 1st check kit, 2nd check kit, or relief kit to repair the part you need.
Check with the local water company to see which kind of backflow preventer you need. It's the water company that determines what they require from you — so they'll usually tell you what you need.
The water company also determines who needs a backflow in addition to what type — not every facility needs one. And it's important to note that each water company has their own rules for determining this, so always check before you purchase property.
There are three different categories that your facility can fall under when it's being checked to see what backflow is good. Your water company determines this.
  • Hazardous — you are hazardous if your facility is close to a pond, river, or ocean or if there are any chemicals that enter your water supply at any time. You'll typically need an RPZ.
  • Aesthetically objectionable — if you're using a sprinkler system with no chemicals, this is typically low hazard. You will typically need a double check valve for this.
  • Non-hazardous — if it is determined that your facility poses no hazard to the public water supply, it will be deemed non-hazardous and you will most likely not need a backflow preventer.
Pressure vacuum breakers are for internal isolation — not external isolation. They do not protect the outside but can be used to internally isolate something in your facility such as a coffee machine, ice maker, etc. An anti-siphon valve is a type of vacuum breaker.
You must follow the instructions on the backflow preventer and all backflow preventers must be tested yearly by a certified tester.
We're Here To Help!
Available 9am
Available 9am
Response by Mon
Response by Mon

Closed Now:
Hours

MondayThursday
8am7:45pm
Friday
9am7:45pm
SaturdaySunday
9am5:45pm
Footer People Non TradeMasterFooter People Non TradeMaster
Give Us Feedback
We'd love to hear about your experience with us.
TAKE SURVEY
Subscribe for More
Stay in the know with top brands & product spotlights!
App Image
Download Our App!
Easier and faster shopping on our 200,000+ products.  SupplyHouse App
© 2026 SupplyHouse.com
Google SellerBBB Reliability SealReseller RatingsPHCC