Eemax has manufactured tankless electric water heaters for more than 30 years and is headquartered in Montgomery, Alabama. The company is now part of Rheem, giving its point-of-use and commercial product lines backing from one of the larger names in water heating manufacturing. Eemax focuses specifically on electric tankless technology rather than tank-style storage water heaters. Its equipment suits spots where a dedicated hot water source at the point of use solves a problem a central tank can't.
Product Lines
Eemax's residential lineup includes the AutoBooster, HomeAdvantage II, and the compact MiniTank. On the commercial side, the catalog covers AccuMix II, FlowCo, LavAdvantage, ProSeries, ProSeries XTP, SafeAdvantage, and SpecAdvantage, along with three-phase models across the Series Two and Series Three lines. The ProSeries XTP delivers output temperatures up to 180 degrees Fahrenheit with flow rates ranging from 0.5 to 20 gallons per minute, suited to higher-demand commercial applications.
Why Contractors Specify Eemax
Point-of-use tankless units cut the pipe run between the heater and the fixture. This reduces the wait for hot water. It also reduces the standby losses that come with a central tank sitting idle. Commercial-focused lines like LavAdvantage target handwashing stations specifically, while FlowCo and AccuMix II address mixed-output commercial applications. Eemax lists membership with organizations including ASPE, AIA, NESEA, and USGBC, which contractors working on plumbing-code-driven commercial jobs may find relevant when specifying equipment.
How to Choose Eemax Products
Sizing an Eemax unit starts with the required flow rate and the temperature rise needed for the application. Electric tankless output is tied directly to incoming water temperature and the amperage available at the panel. Residential single-fixture jobs generally call for smaller units like the MiniTank or HomeAdvantage II, while multi-fixture or high-demand commercial settings point toward the ProSeries or ProSeries XTP line. Three-phase models in the Series Two and Series Three lines fit commercial electrical services that residential single-phase units can't run on. Confirming available amperage and voltage before selecting a model prevents a mismatch between the heater and the electrical service on site.
Frequently Asked Questions
What temperature and flow rate can the Eemax ProSeries XTP handle?
The ProSeries XTP outputs water up to 180 degrees Fahrenheit with flow rates from 0.5 to 20 gallons per minute.
Is Eemax still an independent manufacturer?
Eemax is now a Rheem brand, though it continues to focus specifically on tankless electric water heaters.
What's the difference between Eemax's residential and commercial lines?
Residential models like the AutoBooster, HomeAdvantage II, and MiniTank serve single-fixture home applications. Commercial lines such as ProSeries, FlowCo, and the three-phase Series Two and Series Three models handle higher-demand or multi-fixture settings.
Does Eemax make a model built for handwashing stations?
LavAdvantage is built specifically for handwashing applications.
What professional organizations is Eemax affiliated with?
Eemax lists membership with ASPE, AIA, NESEA, and USGBC.